Join our free process automation webinars

Ask questions, get answers!

Join us for our free webinars covering a range of process automation topics. It’s your chance to find out more and chat directly with our experts!

Benefits

  • Live and interactive – our experts are on hand to answer your questions.

  • Our free webinars can be easily accessed at your convenience.

  • With a wide range of topics, you’re sure to find a subject to suit!

May

Raman Spectrograph for LNG streams - 22 May 2020 >>> Gas Chromatograph requires the use of a vaporizer to convert the liquid sample to a gas prior to measurement. Raman analyzers can measure LNG in the cryogenic liquid state, eliminating the need for vaporization of the sample. Measurement in the liquid phase results in significant reduction in measurement uncertainty time and requires no consumables. How this technology works, and it’s benefits for LNG streams will be discussed.

©Endress+Hauser

Steam in Oil & Gas industry - 26 May 2020 >>> Steam is an expensive necessity for refineries and the upstream Oil & Gas industry. Endress+Hauser has developed many instruments to measure both quality and quantity of steam. This webinar will address the issues and remedies of measuring steam in harsh and explosion dangerous environments.

©Endress+Hauser

Safe, cost effective and accurate metering solutions for custody transfer, metering, injection and production applications - 28 May 2020 >>> Discover the benefits when partnering with Endress+Hauser in your skid design and fabrication project. We'll also talk about our cutting edge ultrasonic gas flowmeter which we have showcased in our demonstration skid, the Prosonic Flow G, and the new benefits it brings in challenging wet gas applications.

©Endress+Hauser

Multipoint temperature in Oil & Gas industry - 28 May 2020 >>> Measuring safely and reliably the temperatures of reactors in refineries but also in LNG storage tanks is critical. Hydrogen permeation during the refinery transformation processes or leaks for LNG storage farms might lead to blind process control or a catastrophe. This webinar will address the problem area’s and the solutions of multipoint temperature systems in the Oil & Gas market.

June

©Endress+Hauser

Water preparation for steam generation in Ex environments - 02 June 2020 >>> The preparation of water before it is turned into steam is essential. It could lead to dangerous failures in the piping and boiler itself. This can lead to less efficiency en eventually catastrophic failure. This webinar will explain what is essential to measure in the boiler makeup water and how, using a leading Oil &Gas company as example.

©Shutterstock

Trace moisture measurement with TDL technology - 04 June 2020 >>> A natural gas liquefaction process comes to a complete stop if the moisture content in LNG streams are not in the PPB levels before it enters the cooling boxes. But how do you measure PPB level moisture in a continuous process reliably and continuously? This webinar will compare technologies, benefits and disadvantages

©iStockphoto/Strandperle

Separators - comparison between Gamma, guided wave radar and capacitance - 09 June 2020 >>> Measuring the oil/water/sand/emulsion layers in separators is not easy. Many technologies are available that all have advantages and disadvantages. This webinar will go through several of them and compare their measurement results.

©Endress+Hauser

Gas volume measurement using Ultrasonic measurement G300 - 11 June 2020 >>> Measuring gas flows with Ultrasonic gas flow meters is not new. The technology however has developed and can offer way more information than just the “gas flow”. This webinar will focus on the latest Ultrasonic developments and the additional information that has now made available, in order to optimize Oil & Gas industry processes and be sure that what you measure is correct and validated.

©Endress+Hauser

Master meter calibration for flowmeters - 16 June 2020 >>> Proving of flowmeters in the Oil & Gas industry is critical. Especially when they are being used as the cash register between buying and selling partners of crude oil, oil-based products and gas. Learn about the advantages of Coriolis master meters over other methods for frequent proving of custody metering points and the level of achievable measuring uncertainty and the potential of reducing costs & risks for frequent proving.